cancel
Showing results for 
Search instead for 
Did you mean: 

Basic Simple ADC use on STM32G0 to measure 0-3.3 thermistors ...

JD3
Associate II

STM32G0B1CBT6

 

#define ADC0_OBJ_COUNT 9

const uint8_t ch_remap[ADC0_OBJ_COUNT] = {ADC_CHANNEL_0, ADC_CHANNEL_1, ADC_CHANNEL_2, ADC_CHANNEL_3, ADC_CHANNEL_4, ADC_CHANNEL_5, ADC_CHANNEL_6, ADC_CHANNEL_7, ADC_CHANNEL_10};

//const uint8_t ch_remap[ADC0_OBJ_COUNT] = {0 , 1, 2, 3, 4, 5, 6, 7, 10};

uint32_t adc1_value[ADC0_OBJ_COUNT];

 

 

static void MX_ADC1_Init(void) {

ADC_ChannelConfTypeDef sConfig = {0};

 

hadc1.Instance = ADC1;

hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;

hadc1.Init.Resolution = ADC_RESOLUTION_12B;

hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;

hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;

hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;

hadc1.Init.LowPowerAutoWait = DISABLE;

hadc1.Init.LowPowerAutoPowerOff = DISABLE;

hadc1.Init.ContinuousConvMode = DISABLE;

hadc1.Init.NbrOfConversion = 1; // 1 konverze najednou

hadc1.Init.DiscontinuousConvMode = DISABLE;

hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;

hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

hadc1.Init.DMAContinuousRequests = DISABLE;

hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;

hadc1.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_160CYCLES_5;

hadc1.Init.SamplingTimeCommon2 = ADC_SAMPLETIME_160CYCLES_5;

hadc1.Init.OversamplingMode = DISABLE;

hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_LOW;

 

if (HAL_ADC_Init(&hadc1) != HAL_OK) {

Error_Handler();

}

 

// Inicializujte první kanál jako výchozí

sConfig.Channel = ADC_CHANNEL_0;

sConfig.Rank = ADC_REGULAR_RANK_1;

sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1;

if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) {

Error_Handler();

}

}

 

void adc1_update(void) {

ADC_ChannelConfTypeDef sConfig = {0};

 

for (uint8_t i = 0; i < ADC0_OBJ_COUNT; i++) {

/* Configure Regular Channel: add channel to sequence */

sConfig.Channel = ch_remap[i];

sConfig.Rank = ADC_RANK_CHANNEL_NUMBER;

//sConfig.SamplingTime = ADC_SAMPLINGTIME_COMMON_1;

HAL_ADC_ConfigChannel(&hadc1, &sConfig);

 

// Spustíme konverzi

HAL_ADC_Start(&hadc1);

HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);

adc1_value[i] = HAL_ADC_GetValue(&hadc1);

adc_obj[i].curr = kalman_filter(&kalman_filters[i], adc1_value[i]);

 

/* Configure Regular Channel: remove channel from sequence */

sConfig.Channel = ch_remap[i];

sConfig.Rank = ADC_RANK_NONE;

HAL_ADC_ConfigChannel(&hadc1, &sConfig);

}

}

 

 

Where is mistake ? It measures only CH0 and copies to all buffer spaces 0-8. I would like to used DMA which works fine, but DMA can do 8 ch RANKS only  i need 16 channels in future slow measuring of resitors

2 REPLIES 2
Karl Yamashita
Lead III

Use the </> icon when posting code so it's properly formatted and readable.

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

Cube/HAL is open source, so you can debug it as your own code. Read out and check/post ADC registers content before you start the individual conversions. 

JW