2020-04-30 4:44 PM
Hello
This is my first time soldering a MCU on a custom PCB.
As you know, STM32f767 is a very complicated chip and requires Vdd and Vss on many pins. Datasheet also states that capacitors are mandatory on each Vdd or Vref+. However Vref and Vdd (marked on figure) are neighbors and I was wondering if I can use one capacitor for both of them.
Could you also tell me if this is a proper way of placing capacitors ? Max distance from Vdd line and cap is 8mm.
As you can see, there is only one track and its obviously Vdd line.
Of course I am not done with placing all caps and tracking Vdds to pins. I first need to know if this kind of principle is going to work
Solved! Go to Solution.
2020-04-30 7:23 PM
Your images show up.
You will find many different opinions on how to place decoupling caps. In general, the closer the better.
Using the same cap for VREF+/VDDA seems fine, unless you want to really optimize ADC noise performance.
Take a look at ST's own layouts to see how they do things. Here's an example from a Nucleo board so you can see how far the decoupling caps are. Some boards out there have decoupling caps way farther away than this--maybe 1cm or so, and yet the board works fine. It really depends how you're using things.
2020-04-30 4:44 PM
I tried to add images but I guess I do not have permissions yet
2020-04-30 7:23 PM
Your images show up.
You will find many different opinions on how to place decoupling caps. In general, the closer the better.
Using the same cap for VREF+/VDDA seems fine, unless you want to really optimize ADC noise performance.
Take a look at ST's own layouts to see how they do things. Here's an example from a Nucleo board so you can see how far the decoupling caps are. Some boards out there have decoupling caps way farther away than this--maybe 1cm or so, and yet the board works fine. It really depends how you're using things.
2020-05-02 8:51 AM
It should be noted that the shown physical layout of PCB traces is pretty wrong!
2020-05-02 1:25 PM
thanks for letting me know that.
However, since I am using only single layer and rails are very thick and rather straight, I dont think it will have that much inductance and resistance.
For time being. I will go with this layout. However, if it does not work I will try to do what was suggested. I will post feedback