cancel
Showing results for 
Search instead for 
Did you mean: 

To build multiple STM32 MCU boards and able to be flashed from a host

WaiSiang
Associate II

Hi,

could share a proper way in the following scenario?

1. How do we design customized boards developed from Nucleo series, and still be able to flash it properly without wiring hassle or ST-link module? Is there a ST reference circuit available? What name does it call?

 

2. If I will have 80 to 100 same STM32F767 based units in the hall, I want to flash Hex to them altogether . How to do that? Should we use the CAN and Ethernet? I dont know.
Is there a professional way to do that?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III

Start with AN2606 or create own custom bootloader