2024-03-18 10:10 PM
Hi everyone, I'm using STM32F429ZI with LAN8742A PHY. Once I start the MCU Ethernet communication works properly, After sometime netif link goes down and ping stops.
Only when I resets the MCU communication starts.
After debugging further it is observed that, Whenever link status updates it goes into ethernetif_Update_config callback function. But autonegotiation processes not completing there and goes into error.(refer below code.)
void ethernetif_update_config(struct netif *netif)
{
__IO uint32_t tickstart = 0;
uint32_t regvalue = 0;
if(netif_is_link_up(netif))
{
/* Restart the auto-negotiation */
if(heth.Init.AutoNegotiation != ETH_AUTONEGOTIATION_DISABLE)
{
/* Enable Auto-Negotiation */
HAL_ETH_WritePHYRegister(&heth, PHY_BCR, PHY_AUTONEGOTIATION);
/* Get tick */
tickstart = HAL_GetTick();
/* Wait until the auto-negotiation will be completed */
do
{
HAL_ETH_ReadPHYRegister(&heth, PHY_BSR, ®value);
/* Check for the Timeout ( 1s ) */
if((HAL_GetTick() - tickstart ) > 5000)
{
/* In case of timeout */
goto error;
}
} while (((regvalue & PHY_AUTONEGO_COMPLETE) != PHY_AUTONEGO_COMPLETE));
Any suggestions to avoid Autonegotiation timeout in this callback?
2024-03-19 08:06 AM
Hi @Preeti
The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.
Regards,
Billy
2024-03-19 08:19 AM - edited 2024-03-19 08:23 AM
EDIT: my mistake, auto negotiation complete bit is in BSR, so partly disregard the stuff below.
You are reading the wrong register, auto-neg. result is in register SSR (31d), can't remember which bit.
Might be the old HAL bug.
/* Wait until the auto-negotiation will be completed */
...
HAL_ETH_ReadPHYRegister(&heth, PHY_BSR, ®value);
Might still be another problem.
Never take the HAL or Cube stuff for granted, if in doubt check registers of STM32 and external hardware.
2024-03-19 08:27 AM
So, next try...
I found my ethernetif_update_config().
if( netif_is_link_up(pNetIf) ), I completely re-init the STM32's MAC interface (incl. auto-neg start and all the PHY stuff), then call ethernetif_notify_conn_changed(pNetIf).
But you should find out why you lose the connection in the first place.
2024-03-21 12:51 AM
Hello,
First of all thanks for your support
When I disconnect the ethernet cable manually in that case only it is completely re-init the STM32's MAC interface (incl. auto-neg start and all the PHY stuff).
But here we are generating noise purposefully, And in that case when link goes down & try to reconnect. But not it is reconnecting, continuously hitting timeout that's why autonegotiation processes not completing there and goes into error.
BSR Reg values are as bellow :
when link is up and stable: 0x782d
when link not stable (not reconnecting): 0x780d
2024-03-21 12:53 AM
Also I cross checked the connection, all are perfect.
2024-12-06 11:07 AM
Did you find a solution to this issue?