cancel
Showing results for 
Search instead for 
Did you mean: 

AN2606 Rev65 Feb 2025 pattern 11 seems incorrect

Aeh1
Associate III

AN2606_Rev65.jpg

I think the correct one should be nBOOT0_SEL(bit) = 0 as in previous version.

Please verify.

1 ACCEPTED SOLUTION

Accepted Solutions
mÆŽALLEm
ST Employee

Hello,

See also at this thread (Already escalated for verification).

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
mÆŽALLEm
ST Employee

Hello,

See also at this thread (Already escalated for verification).

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

After reading your thread, I believe that U0 should be pattern 11 because RM0503 and in Option bytes in STM32CubeProgrammer show NBOOT_SEL bit 
However document  AN2606 Rev65 pattern 11 in the second condition should change nBoot0_SEL(bit) back to 0 as in previous document version.