2022-04-13 8:04 PM
I'm doing some signal integrity verifications using the STM32H7 IBIS models to determine if I need terminations for connecting my STM32H7 to a HyperRAM memory.
I was a bit surprised with the poor signal integrity I was getting, which I assumed was due to faster edges than expected. I looked a bit deeper in my simulations and noticed that the rise time for the IO was only 160 ps. This is an extremely fast number and I was expecting it to be closer to 1 ns.
The IO is running at 1.8 V with HSLV enabled and the fastest IO speed. The MCU has the UFBGA176+25 package.
Is this 160 ps number realistic?
Solved! Go to Solution.
2022-04-14 9:33 AM
I might actually be having some issue with the simulation tool.
I'm getting essentially identical results when using the io8_hslv_ft_hs_1v8 (high-speed hslv) model vs the io8_hslv_ft_ls_1v8 (low-speed hslv) models.
Same thing when using io8_ft_hs_1v8 (high-speed non-hslv) model vs the io8_ft_ls_1v8 (low-speed non-hslv).
The only difference I seem to get is when I enable/disable hslv.
2022-04-13 11:10 PM
I'd say no, not even in a perfect world without stray capacitance from PCB routing and no load.
But that's just an experienced guess.
Datasheet says at highest speed:
Output high to low level
fall time and output low
to high level rise time
C=10 pF, 1.62 V≤VDD≤2.7 V(4) - 1.9 ns
So maybe your simulation is closer to the truth than I thought - if you don't have any load capacitance in your sim.
2022-04-14 9:33 AM
I might actually be having some issue with the simulation tool.
I'm getting essentially identical results when using the io8_hslv_ft_hs_1v8 (high-speed hslv) model vs the io8_hslv_ft_ls_1v8 (low-speed hslv) models.
Same thing when using io8_ft_hs_1v8 (high-speed non-hslv) model vs the io8_ft_ls_1v8 (low-speed non-hslv).
The only difference I seem to get is when I enable/disable hslv.