after enable external flash mapped, couldn't write to external flash.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-05 2:22 AM
I made a board with ST32H7B0ZBT6, and add a external flash with W25Q128JVS。I found after I enable mapped function, I couldn't write data to external flash any more.
the code with enable mapped func as below:
uint8_t W25Qxx_OSPI_Init(void)
{
OSPI_RegularCmdTypeDef s_command;
uint16_t w25qxx_id;
uint8_t value = W25QxJV_FSR_QE;
if (W25Qxx_OSPI_ResetMemory() != OSPI_OK)
{
return OSPI_NOT_SUPPORTED;
}
if (W25Qxx_OSPI_WriteEnable() != OSPI_OK)
{
return OSPI_ERROR;
}
s_command.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
s_command.FlashId = HAL_OSPI_FLASH_ID_1;
s_command.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
s_command.Instruction = WRITE_STATUS_REG2_CMD;
s_command.AddressMode = HAL_OSPI_ADDRESS_NONE;
s_command.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = HAL_OSPI_DATA_1_LINE;
s_command.DummyCycles = 0;
s_command.NbData = 1;
s_command.DataDtrMode = HAL_OSPI_DATA_DTR_DISABLE;
s_command.SIOOMode = HAL_OSPI_SIOO_INST_EVERY_CMD;
s_command.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
s_command.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_DISABLE;
s_command.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_DISABLE;
s_command.DQSMode = HAL_OSPI_DQS_DISABLE;
if (HAL_OSPI_Command(&hospi1, &s_command, HAL_OSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK)
{
return OSPI_ERROR;
}
#if 0
OSPI_MemoryMappedTypeDef cfg;
cfg.TimeOutActivation = HAL_OSPI_TIMEOUT_COUNTER_DISABLE;
if (OSPI_OK != HAL_OSPI_MemoryMapped(&hospi1, &cfg))
{
return OSPI_ERROR;
}
#endif
if (HAL_OSPI_Transmit(&hospi1, &value, HAL_OSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK)
{
return OSPI_ERROR;
}
if (W25Qxx_OSPI_AutoPollingMemReady(W25QxJV_SUBSECTOR_ERASE_MAX_TIME) != OSPI_OK)
{
return OSPI_ERROR;
}
w25qxx_id=W25Qxx_OSPI_FLASH_ReadDeviceID();
if ( w25qxx_id != W25Qxx_ID)
return OSPI_ERROR;
#if (W25Q256 == W25Qxx_ID)
if (W25Qxx_OSPI_Addr_Mode_Init() != OSPI_OK)
{
return OSPI_ERROR;
}
#endif
return OSPI_OK;
}
If I enable these code:
#if 0
OSPI_MemoryMappedTypeDef cfg;
cfg.TimeOutActivation = HAL_OSPI_TIMEOUT_COUNTER_DISABLE;
if (OSPI_OK != HAL_OSPI_MemoryMapped(&hospi1, &cfg))
{
return OSPI_ERROR;
}
#endif
I will not able to write data to external flash with spi interface. Is there something was wrong?
Solved! Go to Solution.
- Labels:
-
OctoSPI
-
STM32H7 series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-05 6:00 AM
I think that's explictly what I said, yes.
This is the primary way to exit Memory Mapped Mode, and so the HAL_OSPI commands don't return with ERROR or BUSY indicators. Look at what errors the HAL functions return, perhaps even look a the HAL source code.
The MCU is sending commands to the memory device in Memory Mapped Mode, and it can't do this concurently with you sending slow write/erase commands, which need to complete and come ready.
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
‎2024-11-05 3:55 AM
Hello @sheng yang ,
@sheng yang wrote:
I couldn't write data to external flash any more.
This statement is confusing. Do you mean that you was able to write data but it stopped working?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-05 4:13 AM
Correct, you can't send commands to the memory whilst in Memory Mapped mode, you will need to use the HAL_OSPI_Abort() to regain control, and then go back into Memory Mapped when finished
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
‎2024-11-05 5:52 AM
I mean, if I don't mapped the external nor flash, then I can write data to it by HAL_OSPI_xxx releate functions. But if I mapped external flash to memory area 0X90000000 - xxxx, then I couldn't write data to the flash any more.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-05 5:55 AM
Did you mean that I must call
HAL_StatusTypeDef HAL_OSPI_Abort(OSPI_HandleTypeDef *hospi)
function when I want to write data to flash by this function as below
uint8_t W25Qxx_OSPI_WritePage(uint8_t *pData, uint32_t WriteAddr, uint32_t Size)
{
OSPI_RegularCmdTypeDef s_command;
if (W25Qxx_OSPI_WriteEnable() != OSPI_OK)
{
return OSPI_ERROR;
}
s_command.OperationType = HAL_OSPI_OPTYPE_COMMON_CFG;
s_command.FlashId = HAL_OSPI_FLASH_ID_1;
s_command.InstructionMode = HAL_OSPI_INSTRUCTION_1_LINE;
s_command.Instruction = QUAD_INPUT_PAGE_PROG_CMD;
s_command.AddressMode = HAL_OSPI_ADDRESS_1_LINE;
#if W25Qxx_ID==W25Q256
s_command.AddressSize = HAL_OSPI_ADDRESS_32_BITS;
#else
s_command.AddressSize = HAL_OSPI_ADDRESS_24_BITS;
#endif
s_command.AlternateBytesMode = HAL_OSPI_ALTERNATE_BYTES_NONE;
s_command.DataMode = HAL_OSPI_DATA_4_LINES;
s_command.DummyCycles = 0;
s_command.DataDtrMode = HAL_OSPI_DATA_DTR_DISABLE;
s_command.SIOOMode = HAL_OSPI_SIOO_INST_ONLY_FIRST_CMD;
s_command.InstructionSize = HAL_OSPI_INSTRUCTION_8_BITS;
s_command.InstructionDtrMode = HAL_OSPI_INSTRUCTION_DTR_DISABLE;
s_command.AddressDtrMode = HAL_OSPI_ADDRESS_DTR_DISABLE;
s_command.DQSMode = HAL_OSPI_DQS_DISABLE;
s_command.Address = WriteAddr;
s_command.NbData = Size;
if (HAL_OSPI_Command(&hospi1, &s_command, HAL_OSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK)
{
return OSPI_ERROR;
}
if (HAL_OSPI_Transmit(&hospi1, pData, HAL_OSPI_TIMEOUT_DEFAULT_VALUE)
!= HAL_OK)
{
return OSPI_ERROR;
}
if (W25Qxx_OSPI_AutoPollingMemReady(HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != OSPI_OK)
{
return OSPI_ERROR;
}
return OSPI_OK;
}
when I mapped the external flash before ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-11-05 6:00 AM
I think that's explictly what I said, yes.
This is the primary way to exit Memory Mapped Mode, and so the HAL_OSPI commands don't return with ERROR or BUSY indicators. Look at what errors the HAL functions return, perhaps even look a the HAL source code.
The MCU is sending commands to the memory device in Memory Mapped Mode, and it can't do this concurently with you sending slow write/erase commands, which need to complete and come ready.
Up vote any posts that you find helpful, it shows what's working..