2022-06-02 9:59 PM
Hi
I am trying to test STM32H747I-EVAL and LCD
My questions are as belows
( I want to connect each other with RGB connector when I design a circuits for STM32H747 with LCD)
I want to get the example source code.
2. Can I get example codes for STM32H747-EVAL?
let me know the link to get them
2022-06-03 2:39 AM
First of all, the STM32H747I-EVAL is obsolete, but the circuitry is identical to the STM32H757I-EVAL. In both, the LCD is connected via MIPI-DSI, not RGB.
Sample code can be found in the project folder of the repository, either locally in the firmware that can be downloaded with STM32CubeMX or STM32CubeIDE, or in the Github repository.
Does it answer your question?
Regards
/Peter
2022-06-03 5:15 AM
I downloaded example codes
There is not example code for LCD RGB
Can I get example code for LCD RGB?
or Can you let me know how to convert MIPI-DSI to RGB or HDMI?
2022-06-03 5:41 AM
The kit already has an LCD with MIPI-DSI connected via CN15, but you can also work with RGB instead (connector CN20).
However, there is also a MIPI-DSI to HDMI converter called B-LCDAD-HDMI1.
Regards
/Peter
2022-06-03 5:46 AM
For RGB you'd perhaps look at the H743I-EVAL board examples. The whole point of an IC supporting DSI is to avoid wasting 24+ pins on RGB
The H747I-DISCO should allow use of the HDMI adapter B-LCDAD-HDMI1 using the ADV7533
I'd expect TI or others to have DSI-to-RGB
2022-06-06 7:06 PM
Thank you for your help
I saw a schematic of B-LCDAD-HDMI1
There are HSSI_D0 ~ HSSI_D3.
I think HSSI_Dx is DSI_Dx of STM32H747
I have a question.
There are HSSI_D0 to HSSI_D3 in schematic, so There are 4 pairs
But There are DSI_D0 to DSI_D1 in STM32H747, so there are 2 pairs
Is there any problem even if you don't need HSSI_D2 and HSSI_D3
2022-06-07 1:19 AM
Correct, the converter used on the B-LCDAD-HDMI1 can receive its video signal via a maximum of 4 DSI lanes, which, however, do not necessarily have to be used. Its data sheet also mentions in table 6 that "Unused channels should be connected to ground".
The circuit of the STM32H757I-EVAL, which is identical to the STM32H747I-EVAL, now shows exactly this GND connection at DSI_D2 and DSI_D3 via SB31...34.
2023-03-10 1:23 AM
Here you have examples for the STM32H747-EVAL : https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H747I-EVAL/Examples