cancel
Showing results for 
Search instead for 
Did you mean: 

8 simultaneous frequency measurements up to 2MHz on STM32U545REQ

frogrammer
Associate

I am using a STM32U545 Nucleo board with a purpose of measuring up to 8 Square wave frequencies simultaneously averaging between 100KHz to 1.5MHz. I only need to measure frequency with as much as accuracy achievable. Finally, I plan to transfer all the readings over I2C.   

What is the best setup for this case in CubeMX? I have tried to follow Input capture DMA examples online but in my board it is GPDMA1, and setup for it is different than some online tutorials. Any suggestions are welcome.

2 REPLIES 2
ahsrabrifat
Associate II

You can use 16-bit or 32-bit timers (TIM2, TIM5 are 32-bit, which is better for high precision).

I wanted to know is there any Examples where GPDMA is used to measure Frequencies and CubeMX setup.