2022-02-16 6:39 AM
I am interfacing a 5V PWM signal with an STM32F030K6T6 MCU using PB0. According to the datasheet this pin is 5V Tolerant. In the past, regardless of a pin's "tolerance" to 5V I have always used a level shifter to change this 5V signal to a 3.3V signal before it gets to the MCU; "Just to be safe". This application I am trying to limit the number of parts on the PCB for both size and cost reasons. Testing on a Nucleo board seems to work and the MCU seems to tolerate this well, but for long term use in the field is it better to run this signal through a level shifter or does it not matter since the pin is "5V Tolerant"?
Solved! Go to Solution.
2022-02-16 7:03 AM
As long as you operate the GPIO as a digital input and switch off its pull-up and pull-down, it can process 5V signals.
Does it answer your question?
Regards
/Peter
2022-02-16 7:03 AM
As long as you operate the GPIO as a digital input and switch off its pull-up and pull-down, it can process 5V signals.
Does it answer your question?
Regards
/Peter
2022-02-16 7:18 AM
The chip needs to be powered in order to be 5V tolerant, but if you can guarantee the chip won't see 5V unless it's powered, there are no issues.
2022-02-16 7:20 AM
Yes, this answers my question. I am not using any internal pull up or pull down resistor on this pin. It is only being setup as a GPIO Input in external interrupt mode:
2022-02-16 7:20 AM
the 5V signal won't damage the MCU over time?
2022-02-16 7:23 AM
No.
2022-02-16 8:02 AM
As long as the device is powered while 5 V applies!
2023-09-27 3:28 PM
2023-09-27 3:31 PM
Sorry, you were right by "switch off", which means disable.
2023-12-15 8:09 PM - edited 2023-12-15 8:10 PM
Hello @Peter BENSCH & @TDK ,
It may seem redundant - but to confirm can we interface a 5V UART Input signal to the UART Rx pin which is 5V tolerant ie FT? As UART is Push-Pull assuming the Pull-up & Pull-down are disabled by default & the GPIO is configured as input only. Any other things to be aware of? The maximum speed shall be upto 4Mbps.