cancel
Showing results for 
Search instead for 
Did you mean: 

32H7 Board Not Connecting - "No STM32 Target Found" Error

Harsh_Gajjalwar
Associate II

I am facing an issue where my STM32H7 board is not detected using STM32CubeProgrammer. I am using an STLINK-V3SET programmer, and the following error keeps appearing:

 

Error log:

17:04:59 : UR connection mode is defined with the HWrst reset mode
17:04:59 : ST-LINK SN : 0028001E3233510739363634
17:04:59 : ST-LINK FW : V3J13M4B5S1
17:04:59 : Board : STLINK-V3SET
17:04:59 : Voltage : 3.29V
17:04:59 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

17:06:59 : UR connection mode is defined with the HWrst reset mode
17:06:59 : ST-LINK SN : 0028001E3233510739363634
17:06:59 : ST-LINK FW : V3J13M4B5S1
17:06:59 : Board : STLINK-V3SET
17:06:59 : Voltage : 3.29V
17:06:59 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

 

Setup Details

  1. Board: STM32H745xi series
  2. Debugger: STLINK-V3SET
  3. Software: STM32CubeProgrammer 
  4. Voltage: 3.3V confirmed

 

Any help or suggestions would be greatly appreciated. Thanks in advance!

 
2 REPLIES 2

@Harsh_Gajjalwar wrote:

 my STM32H7 board 


What board?

Please give details; also versions, etc: How to write your question to maximize your chances to find a solution

TDK
Guru

Has it ever worked or is this a brand new board/design? Are SWD/NRST pins connected? Show schematic, details.

If you feel a post has answered your question, please click "Accept as Solution".