2024-12-17 03:40 AM
I am facing an issue where my STM32H7 board is not detected using STM32CubeProgrammer. I am using an STLINK-V3SET programmer, and the following error keeps appearing:
Error log:
17:04:59 : UR connection mode is defined with the HWrst reset mode
17:04:59 : ST-LINK SN : 0028001E3233510739363634
17:04:59 : ST-LINK FW : V3J13M4B5S1
17:04:59 : Board : STLINK-V3SET
17:04:59 : Voltage : 3.29V
17:04:59 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
17:06:59 : UR connection mode is defined with the HWrst reset mode
17:06:59 : ST-LINK SN : 0028001E3233510739363634
17:06:59 : ST-LINK FW : V3J13M4B5S1
17:06:59 : Board : STLINK-V3SET
17:06:59 : Voltage : 3.29V
17:06:59 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
Any help or suggestions would be greatly appreciated. Thanks in advance!
2024-12-17 03:55 AM
@Harsh_Gajjalwar wrote:my STM32H7 board
What board?
Please give details; also versions, etc: How to write your question to maximize your chances to find a solution
2024-12-17 06:16 PM
Has it ever worked or is this a brand new board/design? Are SWD/NRST pins connected? Show schematic, details.