2017-12-15 05:40 PM
Hello!
I am working with CS43L22 on STM32F407VG Discovery Board.
I use Audio_playback_and_record example to play .wav file.
If i use headphone, I can get good sound. But If I use speaker I get small sound.
Is that normal?
#audio #cs43l222017-12-18 06:14 AM
Hello
quoc.anh
,This can be caused by software configuration issue.
Weneed few more details on your software configuration about used speaker output.Best Regards
Imen
2017-12-18 07:34 AM
Aren't the speaker outputs of CS43L22 unconnected on the STM32F407VG Discovery Board?
JW
2017-12-18 09:29 PM
Yes. I was consider STM32F407 Discovery schematic and CS43L22 Datasheet. You are right! Thanks you for your confirmation.
2017-12-18 09:37 PM
Now I can play wav file into my micro sd card. But I only can play 16bit wav file. I want to play 8bit wav file. How can I do that?
If you need, I can upload my project ! I expect that you can help me !
2017-12-19 12:04 AM
I am not going to review your project and it's unlikely anybody will, but generally, you read 8-bit samples instead of 16-bit from the file, and then you have to shift them to the left by 8 ( << 😎 before using them just like in the 16-bit case.
JW
2017-12-19 01:51 AM
How can I get 'stm32_audio_vocoders_package' ? I read this document
2017-12-19 02:11 AM
Hello
quoc.anh
,As mentioned in the AN4229:'The vocoder firmware package is provided upon request, for more details please contact your local ST sales representative.'
So, you can contact a local ST sales representative from the list indicated at this
http://www.st.com/content/st_com/en/contact-us.html
.
Best Regards,
Imen.