cancel
Showing results for 
Search instead for 
Did you mean: 

Isn't this a mistake

konsul41
Associate II

Sorry, Google Translate changed my previous post to Polish. That's probably why no one answered me.
Now the post is correct.

 

This code was generated by STM322CubeIde

 

 

UINT MX_USBX_Device_Init (VOID *memory_ptr)

{

UINT ret = UX_SUCCESS;

UCHAR *pointer;

TX_BYTE_POOL *byte_pool = ( TX_BYTE_POOL *)ptr_memory;

 

/* BEGIN USER CODE MX_USBX_Device_Init0 */

 

/* USER CODE END MX_USBX_Device_Init0 */

 

/* Allocate stack for main device application thread */

if (tx_byte_allocate(byte_pool, (VOID**) &pointer, UX_DEVICE_APP_THREAD_STACK_SIZE,

TX_NO_WAIT) != TX_SUCCESS)

{

/* USER CODE BEGIN MAIN_THREAD_ALLOCATE_STACK_ERROR */

return TX_POOL_ERROR;

/* USER CODE END MAIN_THREAD_ALLOCATE_STACK_ERROR */

}

 

/* Create the main device application thread */

if (tx_thread_create(&ux_device_app_thread, UX_DEVICE_APP_THREAD_NAME, app_ux_device_thread_entry,

0, pointer, UX_DEVICE_APP_THREAD_STACK_SIZE, UX_DEVICE_APP_THREAD_PRIO,

UX_DEVICE_APP_THREAD_PREEMPTION_THRESHOLD, UX_DEVICE_APP_THREAD_TIME_SLICE,

UX_DEVICE_APP_THREAD_START_OPTION) != TX_SUCCESS)

{

/* USER CODE BEGIN MAIN_THREAD_CREATE_ERROR */

return TX_THREAD_ERROR;

/* USER CODE END MAIN_THREAD_CREATE_ERROR */

}

 

/* BEGIN USER CODE MX_USBX_Device_Init1 */

 

/* USER CODE END MX_USBX_Device_Init1 */

 

return

}

 

 

The problem is that this is an initialization and the main thread is created, but

Then there is the code in the _txe_byte_allocate function

 

TX_THREAD_GET_CURRENT(wątek_ptr);

 

Of course thread_ptr is always equal to 0x0,
which is logical since there is no thread yet.
the problem comes later

 

basen_ptr -> tx_byte_pool_owner = wątek_ptr;
work_ptr = _tx_byte_pool_search(pool_ptr, rozmiar_pamięci);
//work_ptr = 0x0

 

next

if (work_ptr != TX_NULL),

 


which ends up with .refusing to allocate memory


status = TX_NO_MEMORY;

 

 

Is this normal? Maybe I'm generating something wrong?

 

 

 

 

 

 

 

1 REPLY 1
FBL
ST Employee

Hi @konsul41 

It seems like 

/* No memory of sufficient size was found... */

Try to increase the heap/stack size. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.