2024-07-25 2:57 AM
Hi all!
I'm creating a pack using the Pack Creator. My pack uses a BSP template. I've tried creating projects using the pack for a selection of boards. In all cases bar the H5 the pack template successfully creates the right #include for the platform BSP.
I.e. the template uses:
#include "${BoardName}_bus.h"That creates the following:
Board | Created #include |
| L4 Nucleo32 |
#include "stm32l4xx_nucleo_bus.h" |
| H7 Nucleo144 | #include "stm32h7xx_nucleo_bus.h" |
| H5 Discovery Kit | #include "stm32h573i_dk_bus.h" |
| U5 IoT Discovery Kit | #include "b_u585i_iot02a_bus.h |
The correct #include for the H5 board should be:
"stm32h573i_discovery_conf.h"
Short of writing an exception within my template specifically for the H5 discovery board, is there a mistake I'm making with using `BoardName` for my template?
Second question, are there other boards for which `BoardName` wouldn't work?