2024-07-25 2:15 AM - last edited on 2024-07-25 3:11 AM by Andrew Neil
Hello,
because of my mistake, I had assigned the same label for two different pins within CubeMX 6.12. It seems, CubeMX recognize this, but send not an error oder a warning message about it.
What happen, CubeMX is attaching the port- and pinname to the label and renames silent the label. I would expect, a message box is popping up to select, what should be done, e.g.
a. accept the new name or reject
b. correct the label with a new own name
c. inform about the things, went in the background
Section from main.h
#define P5VINT_ENAE7_Pin GPIO_PIN_7       
#define P5VINT_ENAE7_GPIO_Port GPIOE
#define P5VINT_ENA_Pin GPIO_PIN_13
#define P5VINT_ENA_GPIO_Port GPIOI
Thanks,
Jan
2024-07-25 2:55 AM
Hello @JPiet.3
Thank you for your suggestion. I will escalate it to the concerned team so they may consider it in one of the comming releases of STM32CubeMX.
Your contribution is always welcome.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.