Skip to main content
Jan Humpl
Associate
Sep 1, 2017 2:21 PM UTC
Question

STM32CubeMX Feature request: possibility to specify relative paths or our own paths.

Posted on September 01, 2017 at 16:21

Hello,

we want to set path for 'Mcu and Firmware Package' to path relative to CubeMX project directory. Rationale - in case you store CubeMX and other source files into VCS, the absolute path to the Firmware package may be different on each computer. The relative path is always same.

We also want to set 'Toolchain Folder Location' - now this field is not editable.

Thanks a lot.

    This topic has been closed for replies.

    5 replies

    ST Technical Moderator
    Sep 4, 2017 9:13 AM UTC
    Posted on September 04, 2017 at 11:13

    Hello

    jan.humpl

    Thank you for your participation. Iwill raise your request internally to the CubeMx team.

    Best Regards

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Jeanne Joly
    Associate
    Jan 30, 2018 9:11 AM UTC
    Posted on January 30, 2018 at 10:11

    Hello

    jan.humpl

    ,

    In the latest CubeMX release (CubeMX4.24), open File/Project Settings, the toolchain folder can be changed and for the Firmware location, you can untick the button ''Use Default Firmware Location'' and set the path you want :

    0690X00000609XhQAI.png

    I hope it will help you.

    BR. Jeanne

    Jan Humpl
    Jan HumplAuthor
    Associate
    Jan 30, 2018 10:23 AM UTC
    Posted on January 30, 2018 at 10:23

    The behavior is identical to previous version. I cannot set path relative to the current directory (e.g. '..\..\..\..\3party\STM32Cube_FW_H7'). If I try to set relative path I will get this error:

    0690X00000609UtQAI.png

    But the message is not true - I am sure that the folder contains mentioned directories.

    Jeanne Joly
    Associate
    Jan 30, 2018 11:02 AM UTC
    Posted on January 30, 2018 at 11:02

    Please, have a look to

    http://www.st.com/content/ccc/resource/technical/document/user_manual/10/c5/1a/43/3a/70/43/7d/DM00104712.pdf/files/DM00104712.pdf/jcr:content/translations/en.DM00104712.pdf

     doc, paragraph 5.8.1 Project tab, you will have an explanation on how to reuse the same Drivers folder across all projects that use the same firmware location.

    It should help you.

    BR. Jeanne