cancel
Showing results for 
Search instead for 
Did you mean: 

Are the STM32F1/F4/F7/H7 series MCUs suitable for the safety critical system design in Industry Automation?

JWang.8
Associate

Are the STM32F1/F4/F7/H7 series MCUs  and X-CUBE-STL certified for SIL2/3? For a new product design, what's guideline for the hardware design with the SIL Functional Safety Package?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Jack Peacock_2
Senior III

ARM makes controller cores specifically designed for what you describe. Look at the ARM R series. There are several manufacturers.

To answer your question, would you buy a car with the braking system running on a single M series controller?

Jack Peacock

Amel NASRI
ST Employee

Hi @JWang.8​ ,

X-CUBE-STL package is described as following in DB3595:

On the basis of the ST Quality foundations, the STM32 microcontrollers portfolio and the STM32 embedded

safety features, the STM32 SIL functional safety design package helps users to market STM32-based safety

critical applications quickly, targeting the industry safety standard IEC 61508 safety integrity level (SIL2/SIL3) in

domains such as industrial, motor control, factory automation, or power generation/conversion.

The package helps end-users to target safety applications according to various safety standards such as

ISO 13849, IEC 62061 and IEC 61800.

In this page, you can find:

Hope this will be helpful for you, even if it is a late answer.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.