2024-01-16 11:53 PM
I'm finalizing the design of a BLDC motor controller (up to 48V / 40A) and I'd like it to work well with HSO and (when available) ZeST.
From other forum posts I've found the need for phase voltage measuring and to be able to capture these simultaneously. The board already on the face of it the current board config looks compatible:
Questions:
Solved! Go to Solution.
2024-01-19 05:53 AM
Hello,
Please find below the answers to your question:
1. This ADC configuration should be compatible with HSO/ZeST
Regarding the filtering, you can refer to https://www.st.com/en/evaluation-tools/steval-lvlp01.html and https://www.st.com/en/evaluation-tools/b-g473e-zest1s.html which is a pack designed to use HSO/ZeST.
2. In the pack there is a 328KHz cut-off frequency for phase current.
3. 500Hz cut-off frequency is OK for phase voltage sensing. In the pack, it is 518Hz.
Best regards
2024-01-19 05:53 AM
Hello,
Please find below the answers to your question:
1. This ADC configuration should be compatible with HSO/ZeST
Regarding the filtering, you can refer to https://www.st.com/en/evaluation-tools/steval-lvlp01.html and https://www.st.com/en/evaluation-tools/b-g473e-zest1s.html which is a pack designed to use HSO/ZeST.
2. In the pack there is a 328KHz cut-off frequency for phase current.
3. 500Hz cut-off frequency is OK for phase voltage sensing. In the pack, it is 518Hz.
Best regards
2024-01-19 11:36 AM
Thank you for the clear answers!
2024-02-16 04:46 PM
Hi StefanH!
In your post you mentioned: "From other forum posts I've found the need for phase voltage measuring and to be able to capture these simultaneously."
What post did you find that in? Is there a general design guide to creating custom power stages? Any pointers would be appreciated 🙂