cancel
Showing results for 
Search instead for 
Did you mean: 

High power BLDC controller

sshin.9
Associate II

Hello Team,

  We want to develop a BDLC driver with high power. We went through the below product, it matches other requirements except for output current, it is only up to 1.5A

Motor Control Nucleo Pack with NUCLEO-G431RB and X-NUCLEO-IHM16M1

can u suggest a similar module that can support high voltage of up to 60V and a current of up to 20A.

it should be able to operate sensored and sensorless  and also on encoder feedback.

 

Regards,

Sayali

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

You can take a look at the EVSPIN32G4, which should fit your requirements quite well.

 

Good luck!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

You can take a look at the EVSPIN32G4, which should fit your requirements quite well.

 

Good luck!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.