cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-IHM07M1 Motor Driver Board

jerry2
Senior

The Quick Start Guide for this board implies it is compatible only with the following Nucleo boards:

NUCLEO-F030R8

NUCLEO-F103RB

NUCLEO-F302R8

NUCLEO-F401RE

Does anyone know if it will work with any of the Nucleo F7 or H7 boards?

1 REPLY 1
Imen.D
ST Employee

Hello @jerry2​ ,

The X-NUCLEO-IHM07M1 is compatible with STM32 Nucleo boards, with the ST Morpho connector and supports the addition of other boards which can be stacked with onto a single STM32 Nucleo board.

Firstly, you should check if your board is pin to pin compatible with the headers, check the GPIO to enable the motor controller board.

You can adapt the available example (Eg: for NUCLEO-F401RE) to your board.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen