2024-12-23 12:41 AM - last edited on 2024-12-23 01:53 AM by Andrew Neil
Hello everyone!
I was just wondering if I could drive a very high-speed BLDC motor for example a vacuum cleaner one which its nominal speed is 100K rpm using the ST MCSDK.
It doesn't seem doable cuz the max speed when profiling the motor is just only 16000rpm.
is it even possible to run a motor with these specs. using workbench?
what are the solutions? what do you recommend? I really appreciate any help, thanks.