cancel
Showing results for 
Search instead for 
Did you mean: 

UART communication between Hardware and ST motor control workbench

Low Yik Seong
Associate III

Hi, I have encounter a problem when I connect esc001v1 to st motor control workbench monitor through UART. I couldnt connect to ST motor control workbench using UART but I can connect to st motor profiler using UART. I am using SDK 5.2 and IAR workbench IDE to download the program into the esc001v1. So is the problem exist in hardware or in software? Anyway to solve this?

2 REPLIES 2

Hi,

did you have upload the firmware generated with WB 5.2 in the microcontroller before ? Please check if the WB configuration contains the enabling of UART communication. By default it is enabled.

Best regards,

Giuseppe Scuderi

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards