2018-10-09 8:32 AM
Hi, I have encounter a problem when I connect esc001v1 to st motor control workbench monitor through UART. I couldnt connect to ST motor control workbench using UART but I can connect to st motor profiler using UART. I am using SDK 5.2 and IAR workbench IDE to download the program into the esc001v1. So is the problem exist in hardware or in software? Anyway to solve this?
2018-10-15 3:07 AM
Hi,
did you have upload the firmware generated with WB 5.2 in the microcontroller before ? Please check if the WB configuration contains the enabling of UART communication. By default it is enabled.
Best regards,
Giuseppe Scuderi
2021-06-15 1:17 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards