cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX not found - ver. "6.0.0" or higher is required-SOLVED

tarikkutay
Associate

Hi,
I have been getting an error while using MC Workbench to drive ihm03 motor and motor driver package, 
i haven't satisfied by the answers in forum so i solved it in a different way.

At first in installation phase (while setting up STM32CubeMX), i was chosing "Install for me only (recommended)" option for installation mode therefore MCSDK was not to be able to see it from its path.

 

Screenshot 2024-07-02 225420.pngScreenshot 2024-07-02 224920.png

To solve my problem i decided to choose "Install for all users" option. Then now i can generate code in MCSDK.

 

2 REPLIES 2
amina safy
ST Employee

Hello tarikkutay,

Can please tell us in which mode you have installed the MCSDK ?

Thanks 

Amina

 

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
tarikkutay
Associate

Sure Amina,
I have had clicked "Install for anyone using this computer" in MCSDK installer setup.