cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Motor Control - STM32G474xx - HRTIM Support?

GPoll.1
Associate

Hello,

Are there any future plans to add HRTIM Support in ST Motor Contol Workbench?

As far as i have seen G474 is inculded, but only with TIM1 and TIM8. Though these two are the advanced motor control timers, i need a faster PWM signal for my application.

Cheers, G.

1 ACCEPTED SOLUTION

Accepted Solutions
Claire O.
ST Employee

Hello G.,

yes we plan to improve support of STM32G4 in next MCSDK generation. I will check if HRTIM is included as well.

Thanks,

Claire

View solution in original post

2 REPLIES 2
Claire O.
ST Employee

Hello G.,

yes we plan to improve support of STM32G4 in next MCSDK generation. I will check if HRTIM is included as well.

Thanks,

Claire

iskan
Associate III

hello,bro,Did you get your problem solved? Can you share how you solved it?I'm currently experiencing this problem, I'm trying to replace time1 with hrtim in the foc program, can you share? Much appreciated, thanks!