2021-07-03 11:34 PM
STEVAL-PTOOL1V1 , is it support 500 rpm to 12000rpm in three wire BLDC Mode. My motor operate 12v or 24V. i Want to Run this BLDC Motor from 500 rpm to 12000rpm at a PWM or Analog Speed Control.i want to also Direction change and Break. this Board has the features?
Solved! Go to Solution.
2021-07-20 7:00 AM
Hi @senthil,
all the mentioned features can be managed via firmware with the STEVAL-PTOOL1V1 reference design board.
You can find more details in the board user manual UM2770 and firmware example (STSW-PTOOL1V1) user manual UM2771.
The STSW-PTOOL1V1 firmware example features:
I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".
2021-07-04 10:42 PM
Dear @senthil
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools or what version of those tolls you use (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
Best regards
2021-07-04 10:51 PM
Dear @senthil
By the way, STEVAL-PTOOL1V1 is a reference design board. I have no idea about control performances of this board but I add "Motor Control Hardware" topic to your question.
Best regards
2021-07-20 7:00 AM
Hi @senthil,
all the mentioned features can be managed via firmware with the STEVAL-PTOOL1V1 reference design board.
You can find more details in the board user manual UM2770 and firmware example (STSW-PTOOL1V1) user manual UM2771.
The STSW-PTOOL1V1 firmware example features:
I hope this post can help you; if so, consider to mark it as best answer by clicking the label "Select as Best".