2023-08-01 4:08 AM - edited 2023-08-01 4:09 AM
Supply voltage | Nominal | From 10 V to 75 V |
Maximum output current with heatsink (EVSPIN32G4) | Peak | 35 A | |
Continuous(1) | 20 Arms | ||
Maximum output current without heatsink (EVSPIN32G4NH) | Peak | 25 A | |
Continuous(1) | 15 Arms |
Solved! Go to Solution.
2024-01-09 10:58 PM
Hi Kumar,
Not sure what you mean with output voltage. The FET connect the DC supply voltage to the Motor, so the maximum voltage with a PWM dutycycle of 100% is the DC supply voltage.
The switching frequency can be set in the MC Workbench from 2 to 100kHz but is 30kHz by default.
2023-09-14 6:33 AM
Dear Kumar Raja,
Firstly, we would like to sincerely apologize for the delay in replying to your post.
If your point is still pertinent, you can find the full documentation set here: EVSPIN32G4.
The maximum MCU frequency is 170Mhz.
The allowed DC supply voltage is from 10V to 75V.
2024-01-05 8:43 PM
Hi.,
EVSPIN32G4
I am asking only for output Voltage (switching variable voltage ac or dc ) and output switching frequency.
warm Regards
Kumar Raja
2024-01-09 10:58 PM
Hi Kumar,
Not sure what you mean with output voltage. The FET connect the DC supply voltage to the Motor, so the maximum voltage with a PWM dutycycle of 100% is the DC supply voltage.
The switching frequency can be set in the MC Workbench from 2 to 100kHz but is 30kHz by default.