User Activity

  Hello, we're using the EVSPIN32G4 ST evaluation board. in this evaluation Board design with two microcontrollers (stm32f103cbt6 for debugging and STSPIN32G4 for motor control). Unfortunately, the STM32f103cbt6 microcontroller has failed!! We bought...
Motor Control Workbench 6.2.1 I Have using the above version Pilot software. i am getting Speed feedback Err in BLDC Motor application. before i was try Hall Sensor Position Sequence value find and fill it . but i can't solve this fault.  any one sup...
Hi   i have recently purchased for ST Evaluation Board EVSPIN32G4   Supply voltage Nominal From 10 V to 75 VMaximum output current with heatsink (EVSPIN32G4) Peak 35 AContinuous(1)  20 Arms Maximum output current without heatsink (EVSPIN32G4NH) Peak ...
Kudos given to