2021-06-18 01:59 AM
I have created an ESC based on schematic of B-G431B-ESC1 and connected it to my NUCLEO-G431RB board.
Generated software in ST Motor Control Workbench 5.Y for Inverter-B-G431B-ESC1 and changed the MCU to STM32G431RB with all defaults.
The built software on my G431RB nucleo does not work:
Are there any special options ot be set in MCSDK to let it work?
Till now I have no success with the software generated in MCSDK for neither B-G431B-ESC1 (STM32G431RB) nor the EVSPIN32G4 (STSPIN32G4). Behaviour of the µC is always the same.
On a picture in attachment you can see my ESC board.
Thank you in advance.
2021-07-01 08:49 PM
Dear @HAL-9000
When you run MC_MotorControl_Init step by step, where is blocked the SW?
Best regards