cancel
Showing results for 
Search instead for 
Did you mean: 

MC Workbench Sensorless motor Control: motor goes to full speed at start up, desired speed later?

FMaur.1
Associate

Hello,

 

I am driving a motor using the STEVAL-SPIN3201. The code is generated via the mc workbench.

When I test the programm, the motor behaves like that:

The motor starts up slowly according to the start up procedure I chose in the workbench.

Then suddenly the motor moves with fullspeed for some seconds.

After this the motor slowes down to the desired speed. Now I am able to change this speed via the motor pilot.

 

When I change the Kp and Ki value, I can reduce the duration of the "full speed periode". However, it is still there.

 

Can you explain what is happening and why the motor moves to full speed for a short time?

 

Thanks a lot for your help!

Florian

2 REPLIES 2
Cristiana SCARAMEL
ST Employee

Since your question is about STM32 MCSDK, I added STM32 Motor Control topic.

If you feel a post has answered your question, please click "Accept as Solution"
cedric H
ST Employee

Hello Florian,

Could you attach your stwb6 project file. (renamed in .txt) ?

Regards

Cedric