2024-04-17 08:55 AM
Hello everybody,
I have a Problem with the X-NUCLEO-IHM07M1 power board . I am using it with the Nucleo-F401RE.
My setup :
Software: Cube IDE + ST Motor control workbench 5.4.8 (I have also tried it with V. 6.2.0)
Motor: Maxon EC i 30 , Art. No 539477 (24V , 2 pole pairs, Hall Sensors)
With the power board X-NUCLEO-IHM08M1 it works . Same setup and software.
For me it is a little bit confusing because X-NUCLEO-IHM08M1 power board is for bigger motors than the Maxon Motor and in my opinion it should work better with the X-NUCLEO-IHM07M1.
If anyone has any ideas about this problem or needs further informations, please let me know.
Here is a screenshot from the motor data sheet.
Parameters workbench:
2024-04-23 01:43 AM
Hello @UNBEEKANNT,
What kind of issue are you facing with X-NUCLEO-IHM07M1?
You mentioned "Same setup and software"; as IHM07 and IHM08 are differents, you should re-generate a project for each power board.
2024-04-23 04:13 AM
Hello @GMA ,
I meant with same software , the same programs(Workbench, motor profiler, cube ide) and same versions of them.
I have two different projects. One for each power board. When using the IHM08 power board, I observed short peaks in the input current, reaching up to 3.5 A(You can see it in the picture below). I have also a voltage drop at the DIA/EN Input of the IC L6230PD, which is used for the board IHM07.
But this signal is never used in the code for the board.
Voltage drop of the DIA/EN Signal measured at PIN CN10/13
Input current for the motor. 100mV = 1 A(Board IHM 07)
Input current for the motor. 100mV = 1 A(Board IHM 08)
I have tried it with and without Hall Sensors,different PWM Frequency ( 5000-25kHz), but nothing works.
If you have any ideas or you need further informations, please let me know.
Thank you for your help.
best regards
UNBEEKANNT 🙂
2024-04-23 05:04 AM
Hello @UNBEEKANNT,
My question about "issue" was more, with IHM07, do you have a reported error? Does the motor spins?
2024-04-23 05:26 AM
I got no reported error and the motor does not spin. The motor just makes half of n cycle and stops there.
I got no error and nothing happens after this short movement.
2024-04-23 05:42 AM
Hello @GMA ,
n addition, I have noticed that the STM workbench shows me a speed on its monitor, but the motor does not move. I had the same problem with the Motor Profiler.
After checking several times, everything is wired correctly. The jumpers are also set correctly.
I also noticed that there is an error when generating code because I am not using Oracle Java8. Could this be related? However, it must also be said that I get this error every time and the motor still turns with the power board "ihm 08, so I thought it could be a software bug.
Greetings
UNBEEKANNT
2024-04-24 05:44 AM
Hello @UNBEEKANNT,
I am able to have such behavior if U and W phases are inverted, did you check Motor phases and Hall sensor connections with IHM07?
Did you try the 5.4.8 motor profiler (with F401+IHM07) to check if motor spins in this case?
2024-04-26 05:25 AM
Hello @GMA ,
I have checked the wiring several times and I also tried it with the power board IHM 08 and with this board the motor spins(same wiring). So I think the wiring is correct.
I have also used the motor profiler and the motor does not spin .
Could the L6230PD be the problem, because the peak of the output current is too high.
Maybe I just need another Motor, which is a little bit smaller.
Greetings
UNBEEKANNT