2024-07-09 4:53 AM - last edited on 2024-07-09 8:54 AM by Andrew Neil
I am using P-NUCLEO-IHM03 motor kit which comprises a STM32G431RB series microcontroller, gimbal motor (GBM2804H-100T), X-NUCLEO-IHM16M1
I am interfacing LM35 temperature sensor to control the speed of the BLDC motor so as the temperature increases (eg. by using a soldering gun) the motor speed is also increasing so the motor is varying its speed according to the change in the ambient temperature but I am not able to print the value of the temperature on the console even though i have given the printing condition and in the live expression the value of the variable that is being displayed is not the right one too there is no proper ADC conversion happening nor I can read the temperature value.
Please help me solving this issue
2024-07-09 8:57 AM
Start by doing just one thing at a time!
@SahanaRaghu wrote:I am not able to print the value of the temperature on the console even though i have given the printing condition
Are you able to print anything at all to this "console" ?
What "console" are you using?
How is this "console" connected to your Target?