MSDK 5.y.4. Incorrect operation of the encoder alignment function.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-05 4:09 AM
Hello,
When working with an incremental encoder, after performing the encoder alignment procedure, it is imperative to perform the function
MC_StopMotor1();
Otherwise, the current (Id ref) is incorrectly set, which can lead to overheating of the motor.
This problem is especially relevant in the position control mode, since in this mode the motor stop function is not used.
Best regards.
Solved! Go to Solution.
- Labels:
-
STM32 Motor Control
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-14 8:59 AM
Hello MK.1
The MC_StopMotor1() is implicit in a sense that at the end of the alignment state the PWM are switched off and restarted when we go to run state. The issue here, in a position control project, is that the call the FOC_Clear(M1) routine (which clears the current references among other things) is missing at the end of the alignment. If you add this call before exiting the alignment state, it should solve your issue.
Best regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-14 8:59 AM
Hello MK.1
The MC_StopMotor1() is implicit in a sense that at the end of the alignment state the PWM are switched off and restarted when we go to run state. The issue here, in a position control project, is that the call the FOC_Clear(M1) routine (which clears the current references among other things) is missing at the end of the alignment. If you add this call before exiting the alignment state, it should solve your issue.
Best regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-14 11:27 AM
Thanks for the reply and advice. I will try to use this. But, on the other hand, I will answer the following:
-the problem is present in all modes, including speed and torque mode
-during the encoder alignment process, the current value (Id ref) should take the value 0, which does not happen. I hope you take this into account in future updates.
Best regards.
ps sorry, I'm using a translator
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-15 7:39 AM
Hi, I was just going to post on this and noticed you had beaten me to it. Glad to confirm this is a bug and not something wrong with my setup. I think this is not new to the latest release either, and yes it affects torque, speed and position control configurations, although you notice it more with position control because the motor is generally not doing anything immediately after the alignment in position control mode.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-15 7:48 AM
That helped. Thanks!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-15 7:55 AM
Hi,
add the following line to the mc.task.c file
/* USER CODE BEGIN MediumFrequencyTask M1 EndOfEncAlignment */
FOC_Clear(M1);
/* USER CODE END MediumFrequencyTask M1 EndOfEncAlignment */
this will solve the problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-16 4:32 PM
Hi, I wonder if it is the same issue for SDK 5.y.3 which I'm using for my project.
In SDK 5.y.3, FOC_Clear(M1) is executed at ANY_STOP state after alignment - is it different in SDK 5,y.4?
=========================================================
case ALIGNMENT:
...
/* USER CODE BEGIN MediumFrequencyTask M1 EndOfEncAlignment */
/* USER CODE END MediumFrequencyTask M1 EndOfEncAlignment */
STM_NextState( &STM[M1], ANY_STOP );
...
case ANY_STOP:
R3_2_SwitchOffPWM( pwmcHandle[M1] );
FOC_Clear( M1 );
================================================================
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-17 12:40 AM
Hi, in version MSDK 5.y.4 the state machine has been changed (simplified). New state machine...
the ANY STOP state machine no longer exists
typedef enum
{
ICLWAIT = 12, /*!< Persistent state, the system is waiting for ICL
deactivation. Is not possible to run the motor if
ICL is active. Until the ICL is active the state is
forced to ICLWAIT, when ICL become inactive the state
is moved to IDLE */
IDLE = 0, /*!< Persistent state, following state can be IDLE_START
if a start motor command has been given or
IDLE_ALIGNMENT if a start alignment command has been
given */
ALIGNMENT = 2, /*!< Persistent state in which the encoder are properly
aligned to set mechanical angle, following state can
only be ANY_STOP */
CHARGE_BOOT_CAP = 16, /*!< Persistent state where the gate driver boot
capacitors will be charged. Next states will be
OFFSET_CALIB. It can also be ANY_STOP if a stop motor
command has been given. */
OFFSET_CALIB = 17, /*!< Persistent state where the offset of motor currents
measurements will be calibrated. Next state will be
CLEAR. It can also be ANY_STOP if a stop motor
command has been given. */
START = 4, /*!< Persistent state where the motor start-up is intended
to be executed. The following state is normally
SWITCH_OVER or RUN as soon as first validated speed is
detected. Another possible following state is
ANY_STOP if a stop motor command has been executed */
SWITCH_OVER = 19, /**< TBD */
RUN = 6, /*!< Persistent state with running motor. The following
state is normally ANY_STOP when a stop motor command
has been executed */
STOP = 8, /*!< Persistent state. Following state is normally
STOP_IDLE as soon as conditions for moving state
machine are detected */
FAULT_NOW = 10, /*!< Persistent state, the state machine can be moved from
any condition directly to this state by
STM_FaultProcessing method. This method also manage
the passage to the only allowed following state that
is FAULT_OVER */
FAULT_OVER = 11, /*!< Persistent state where the application is intended to
stay when the fault conditions disappeared. Following
state is normally STOP_IDLE, state machine is moved as
soon as the user has acknowledged the fault condition.
*/
WAIT_STOP_MOTOR = 20
} MCI_State_t;
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-02-17 2:26 AM
Thank you ! It looks like SDK 5.y.4 has more major changes compared to the small version up.
Regards,
THA.1