User Activity

Hello,When working with an incremental encoder, after performing the encoder alignment procedure, it is imperative to perform the function MC_StopMotor1();Otherwise, the current (Id ref) is incorrectly set, which can lead to overheating of the motor....
CubeMX 6.4.0Cube IDE 1.8MSDK 5.y.4Nucleo -F446REIHM 08M1 3shHello,I noticed that in position control mode, the PID controller generates a current Id ref value other than 0. Is it supposed to be like this? In version MSDK 5.4.8 the current Id referen...
CubeMX 6.4.0Cube IDE 1.8MSDK 5.y.4The new processor load calculation module conflicts in position control mode.
Kudos from