cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Pilot - open loop voltage

Vincent7
Associate II

Hello Everybody,

MCSDK:6.3.0

CubeMX: 6.3.0

Workbench : 6.3.0

Motor Pilot : 1.2.9

I am running on a IHM08M1 with STM32G431, The control is FOC Observer+PLL(sensorless) with 3 shunt.
I want to test the open-loop function of FOC. I have already checked the "open loop" option under "Debug Settings" in the "Drive Settings" page of Workbench. However, when I run Motor Pilot, the "Open Loop - Voltage" control option does not appear in the control menu. Is there anything else I need to configure??

wb6.3.0.png

motor pilot.png

1 ACCEPTED SOLUTION

Accepted Solutions
GMA
ST Employee

Hello @Vincent7,

According to the motor pilot interface, your project has been generated in "profiler" mode. Disable it and generate the project, "Open Loop: Enable" should appear in motor pilot interface.

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

2 REPLIES 2
GMA
ST Employee

Hello @Vincent7,

According to the motor pilot interface, your project has been generated in "profiler" mode. Disable it and generate the project, "Open Loop: Enable" should appear in motor pilot interface.

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
Vincent7
Associate II

Hello GMA, 

Thank you so mucn, the Open Loop-Voltage option has appeared.