cancel
Showing results for 
Search instead for 
Did you mean: 

Installation error of FP-IND-DATALOGMC

hamaogeoge
Associate

STM32CubeFunctionPack_DATALOGMC_V1.1.1をwebからダウンロードし

Downloaded STM32CubeFunctionPack_DATALOGMC_V1.1.1 from the web.

hamaogeoge_1-1731919803763.png


en.fp-ind-datalogmc\STM32CubeFunctionPack_DATALOGMC_V1.1.1\Utilities\HSDPython_SDK\HSDPython_SDK_install.bat
を実行すると

When I run en.fp-ind-datalogmc\STM32CubeFunctionPack_DATALOGMC_V1.1.1\Utilities\HSDPython_SDK\HSDPython_SDK_install.bat
hamaogeoge_0-1731919726745.png



以下のようにエラーが出ます

このエラーを解決したいです。python3.13をインストール済みです。
HSDPython_SDK Installer

I get the following error

I want to resolve this error. I have already installed python3.13.

When I run HSDPython_SDK Installer

[NOTE]: If you are using a proxy launch this script passing your proxy string as a parameter.
-- e.g.: HSDPython_SDK_install.bat http://usr_name:password@proxyserver_name:port#

===========================================
installing st_pnpl...
===========================================
Processing c:\windows\system32\st_pnpl\dist\st_pnpl-2.3.0-py3-none-any.whl
Installing collected packages: st-pnpl
Successfully installed st-pnpl-2.3.0
===========================================
installing st_dtdl_gui...
===========================================
Processing c:\windows\system32\st_dtdl_gui\dist\st_dtdl_gui-2.3.0-py3-none-any.whl
Requirement already satisfied: st-pnpl in c:\users\1022616-z100\appdata\local\programs\python\python313\lib\site-packages (from st-dtdl-gui==2.3.0) (2.3.0)
Collecting numpy==1.26.4 (from st-dtdl-gui==2.3.0)
Using cached numpy-1.26.4.tar.gz (15.8 MB)
Installing build dependencies ... done
Getting requirements to build wheel ... done
Installing backend dependencies ... done
Preparing metadata (pyproject.toml) ... error
error: subprocess-exited-with-error

× Preparing metadata (pyproject.toml) did not run successfully.
│ exit code: 1
╰─> [21 lines of output]
+ C:\Users\1022616-Z100\AppData\Local\Programs\Python\Python313\python.exe C:\Users\1022616-Z100\AppData\Local\Temp\pip-install-5ecukql4\numpy_ceb10f8937c948308aaac2e82576dc45\vendored-meson\meson\meson.py setup C:\Users\1022616-Z100\AppData\Local\Temp\pip-install-5ecukql4\numpy_ceb10f8937c948308aaac2e82576dc45 C:\Users\1022616-Z100\AppData\Local\Temp\pip-install-5ecukql4\numpy_ceb10f8937c948308aaac2e82576dc45\.mesonpy-y40uuct9 -Dbuildtype=release -Db_ndebug=if-release -Db_vscrt=md --native-file=C:\Users\1022616-Z100\AppData\Local\Temp\pip-install-5ecukql4\numpy_ceb10f8937c948308aaac2e82576dc45\.mesonpy-y40uuct9\meson-python-native-file.ini
The Meson build system
Version: 1.2.99
Source dir: C:\Users\1022616-Z100\AppData\Local\Temp\pip-install-5ecukql4\numpy_ceb10f8937c948308aaac2e82576dc45
Build dir: C:\Users\1022616-Z100\AppData\Local\Temp\pip-install-5ecukql4\numpy_ceb10f8937c948308aaac2e82576dc45\.mesonpy-y40uuct9
Build type: native build
Project name: NumPy
Project version: 1.26.4
WARNING: Failed to activate VS environment: Could not parse vswhere.exe output

..\meson.build:1:0: ERROR: Unknown compiler(s): [['icl'], ['cl'], ['cc'], ['gcc'], ['clang'], ['clang-cl'], ['pgcc']]
The following exception(s) were encountered:
Running `icl ""` gave "[WinError 2] 指定されたファイルが見つかりません。"
Running `cl /?` gave "[WinError 2] 指定されたファイルが見つかりません。"
Running `cc --version` gave "[WinError 2] 指定されたファイルが見つかりません。"
Running `gcc --version` gave "[WinError 2] 指定されたファイルが見つかりません。"
Running `clang --version` gave "[WinError 2] 指定されたファイルが見つかりません。"
Running `clang-cl /?` gave "[WinError 2] 指定されたファイルが見つかりません。"
Running `pgcc --version` gave "[WinError 2] 指定されたファイルが見つかりません。"

A full log can be found at C:\Users\1022616-Z100\AppData\Local\Temp\pip-install-5ecukql4\numpy_ceb10f8937c948308aaac2e82576dc45\.mesonpy-y40uuct9\meson-logs\meson-log.txt
[end of output]

note: This error originates from a subprocess, and is likely not a problem with pip.
error: metadata-generation-failed

× Encountered error while generating package metadata.
╰─> See above for output.

note: This is an issue with the package mentioned above, not pip.
hint: See above for details.
===========================================
installing st_hsdatalog (GUI version)...
===========================================
Processing c:\windows\system32\st_hsdatalog\dist\gui\st_hsdatalog-3.3.0-py3-none-any.whl
Requirement already satisfied: st-pnpl in c:\users\1022616-z100\appdata\local\programs\python\python313\lib\site-packages (from st-hsdatalog==3.3.0) (2.3.0)
INFO: pip is looking at multiple versions of st-hsdatalog to determine which version is compatible with other requirements. This could take a while.
ERROR: Could not find a version that satisfies the requirement st-dtdl-gui (from st-hsdatalog) (from versions: none)
ERROR: No matching distribution found for st-dtdl-gui
===========================================
installing asciimatics...
===========================================
Collecting asciimatics
Using cached asciimatics-1.15.0-py3-none-any.whl.metadata (7.1 kB)
Requirement already satisfied: pyfiglet>=0.7.2 in c:\users\1022616-z100\appdata\local\programs\python\python313\lib\site-packages (from asciimatics) (1.0.2)
Requirement already satisfied: Pillow>=2.7.0 in c:\users\1022616-z100\appdata\local\programs\python\python313\lib\site-packages (from asciimatics) (11.0.0)
Requirement already satisfied: wcwidth in c:\users\1022616-z100\appdata\local\programs\python\python313\lib\site-packages (from asciimatics) (0.2.13)
Requirement already satisfied: pywin32 in c:\users\1022616-z100\appdata\local\programs\python\python313\lib\site-packages (from asciimatics) (308)
Using cached asciimatics-1.15.0-py3-none-any.whl (137 kB)
Installing collected packages: asciimatics
Successfully installed asciimatics-1.15.0
続行するには何かキーを押してください . . .

Press any key to continue . . .

1 ACCEPTED SOLUTION

Accepted Solutions
SimonePradolini
ST Employee

Hello @hamaogeoge 

I'm sorry, but Python 3.13 is not supported due to a dependency to PySide6 Python package.

As a consequence, HSDPython_SDK is compatible with Python 3.12 up only.

Can you try the SDK by installing Python 3.12?

 

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
SofLit
ST Employee

Hello @hamaogeoge and welcome to the community,

The language used in this community is English. So please in next time use English as it's a international community.

Thank you for your understanding.

PS: I've added the translation in your post.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
SimonePradolini
ST Employee

Hello @hamaogeoge 

I'm sorry, but Python 3.13 is not supported due to a dependency to PySide6 Python package.

As a consequence, HSDPython_SDK is compatible with Python 3.12 up only.

Can you try the SDK by installing Python 3.12?

 

Best regards

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hello @hamaogeoge 

Any news on the topic? Have you tried with Python 3.12?

 

Best regards,

Simone

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.