cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to know if either or both STEVAL-IHM040V1 and EVSPIN32F06Q1S3 are plug and play modules for controlling 3-Phase Sensorless Motors, and do not require initial software programming?

SBung.1
Associate II
This discussion is locked. Please start a new topic to ask your question.
29 REPLIES 29

Hi,

Yes , Can you share your motor detail as below ?

0693W00000AOwrpQAD.png

Are you able to generate the code ?

Greetings,
I have not yet connected the EVSPIN32F0601S3 to the motor.
Please see the picture of motor below:
Regards,Santos

I have not seen any picture . Please reload .

SBung.1
Associate II

I lost the laptop and have not downloaded the mcsdk on the new laptop yet, but the following inputs that are different from your example above:

Poles Pairs: 6, Nnominal DC Voltage: 400 V.

Further information of the following title from STM32 Motor Control & STM32CubeMX:

Generated Project is showing IPConfigManager:1461 error.

Hi,

1) Can you rewrite what problem(s) you are facing ?

2) Are you able to generate the code successfully ?

--

Karan

SBung.1
Associate II

I will try again once I have the MCSDK running, then will confirm to you.

OK .. I am able to generate/compile the code successfully with MCSDK .

Are you?

--

Karan

Did you get some time?

​Are you able to spin the Motor?

Greetings Karan, thank you for your message, and apologise for my late reply and for not getting the time to spin the motor yet, which for personal issue I will not be able to do so until the month of August.