2021-02-10 03:38 PM
2021-05-19 07:45 AM
Hi,
Yes , Can you share your motor detail as below ?
2021-05-19 07:49 AM
Are you able to generate the code ?
2021-05-19 07:52 AM
2021-05-19 07:54 AM
I have not seen any picture . Please reload .
2021-05-19 08:06 AM
I lost the laptop and have not downloaded the mcsdk on the new laptop yet, but the following inputs that are different from your example above:
Poles Pairs: 6, Nnominal DC Voltage: 400 V.
Further information of the following title from STM32 Motor Control & STM32CubeMX:
Generated Project is showing IPConfigManager:1461 error.
2021-05-19 08:11 AM
Hi,
1) Can you rewrite what problem(s) you are facing ?
2) Are you able to generate the code successfully ?
--
Karan
2021-05-19 08:14 AM
I will try again once I have the MCSDK running, then will confirm to you.
2021-05-19 08:16 AM
OK .. I am able to generate/compile the code successfully with MCSDK .
Are you?
--
Karan
2021-05-27 12:50 PM
Did you get some time?
Are you able to spin the Motor?
2021-06-01 04:43 AM
Greetings Karan, thank you for your message, and apologise for my late reply and for not getting the time to spin the motor yet, which for personal issue I will not be able to do so until the month of August.