cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to know if either or both STEVAL-IHM040V1 and EVSPIN32F06Q1S3 are plug and play modules for controlling 3-Phase Sensorless Motors, and do not require initial software programming?

SBung.1
Associate II
This discussion is locked. Please start a new topic to ask your question.
29 REPLIES 29

Hello Santos,

It is a little bit complicated to describe in a single post how to develop an entire project step by step.

My suggestion is to start reading this guide about the MCSDK (UM2374).

Then, if you have specific questions you should open a different post with the specific question in the title of the post.

Thanks to all the members doing in this way, the ST Community enhances with a list of well-defined questions, structured by topics, so that all the other Community members can easily find a well-defined answers.

Thank you for your contribution.

All the Best !

Thank you for your support Dario, much appreciated!

Greetings Dario,
I need help to Generate Project using EVSPIN32F0601S3.
I am geeting errors when generating the project, concludes with: Completed with Errors.
 
I then attempt to run the STM32CubeMX this start copying libraries files to 70%, then it stops there, no further updates.
 
So if I close the Project Generation, the Workbentch says Generation failed.

Hi

@SBung.1(Community Member),

Are you able to spin the HV motor ? with EVSPIN32F0601S3 and mcsdk.

---

Thanks

Karan​

Greetings Karan​,
No, I am not able to spin the motor still, my case was closed without any support being given.
Thank you for checking on me, I hope you will be able to provided the help I need.
Regards,
Santos

Thanks...

May I know where you stuck ?

Hardware/Software part..​ ?

--

Karan​

Greetings Karan​,
Software problems/errors, I will forward you a separate email to review.
Reagrds,Santos

----- Forwarded message ----- From: Reply to ST Community <xorztlf8h0v6hes3.r2jzd5fc6brmxorb.eh7hu2exio1ilpxl@85rhn7foy9akcdbz.wls6ex2qnci5g.b-ytg6eak.eu28.chatter.salesforce.com

>Sent: Friday, 12 March 2021, 20:30:36 GMTSubject: ...you in group Power Management and Motor Control: I would like to know if either or both STEVAL-IHM040V1 and EVSPIN32F06Q1S3 are plug and play modules for controlling 3-Phase Sensorless Motors, and do not require initial software...?

Greetings Dario,

I need help to Generate Project using EVSPIN32F0601S3.

I am geeting errors when generating the project, concludes with: Completed with Errors.

I then attempt to run the STM32CubeMX this start copying libraries files to 70%, then it stops there, no further updates.

So if I close the Project Generation, the Workbentch says Generation failed.

OK

Greetings again,
Did managed to received the email I forwarded?
Regards,
Santos