Hello ST Community,
I am working with an STM32U585 custom board and I would like to clarify the supported and recommended workflow for flashing TrustZone‑enabled firmware with SBSFU using USB DFU via STM32CubeProgrammer.
Hardware / Software Setup
- MCU: STM32U585
- Custom hardware board
- Tool: STM32CubeProgrammer v2.19.0
- Interface tested:
- Security configuration:
- TrustZone enabled (TZEN = 1)
- SBSFU (Secure Boot & Secure Firmware Update) used
What works (via ST‑LINK / SWD)
Using STM32CubeProgrammer CLI with ST‑LINK, I am able to successfully flash all components:
SBSFU bootloader
- File: SBSFU.bin
- Address: 0x0C004000
Initial SBSFU application image
- File: sbsfu_app_init.bin
- Size: ~1.80 MB (0x1c000)
- Address: 0x0C030000
The script erases the correct flash sectors, programs the binaries, verifies them successfully, and the board boots correctly.
So SWD flashing works as expected for:
- TrustZone‑enabled device
- SBSFU bootloader
- SBSFU application slot
What I am trying to understand (USB DFU case)
After SBSFU and TrustZone are enabled, I tried to flash the same application image using USB DFU via STM32CubeProgrammer.
Observed behavior in CubeProgrammer DFU log:
This indicates that:
- USB DFU bootloader cannot access 0x0cxxxxx secure flash regions
- CubeProgrammer remaps the address to 0x0803xxxx, which is not the SBSFU application slot
My Understanding So Far
From my experiments, it appears that:
- ROM USB DFU:
- Can only access non‑secure flash regions
- Cannot program SBSFU slots (0x0cxxxxx )
- SBSFU‑based DFU:
- Does not allow absolute address programming
- Expects a signed application image
- SBSFU internally decides where to write the image (slot0)
Questions to the Community / ST Team
- Is it supported to flash a TrustZone‑enabled device with SBSFU bootloader entirely using USB DFU via STM32CubeProgrammer (without ST‑LINK)?
- Is the correct approach that ST‑LINK is mandatory at least once (factory provisioning) to install SBSFU and enable TrustZone, and USB DFU can only be used later for signed application upgrades?
- Is it correct that sbsfu_app_init.bin is only meant for SWD provisioning and not for USB DFU updates?
- For USB DFU with SBSFU, should CubeProgrammer be used without specifying any flash address, letting SBSFU handle the internal placement?
- Is there any official ST documentation explicitly stating that SBSFU + TrustZone cannot be initially flashed via USB DFU?