2025-03-07 2:27 AM - last edited on 2025-03-07 2:39 AM by Peter BENSCH
Hello Everybody,
MCSDK:6.3.0
CubeMX: 6.3.0
Workbench : 6.3.0
Motor Pilot : 1.2.9
Power Board : IHM08M1(Rshunt=0.01Ω)
Control Board : NUCLEO-G431RB
Motor : BLDC 26w 24v/8 pole pairs / rpm=4k / rated current=1.8A/hall sensor
I would like to ask, in SPEED MODE under SMO + PLL, which API can be used to limit the Iq current?
For example, if the rated motor current is 2A and the peak current is 6A,
I want to limit the motor's current to not exceed 1.8A during normal operation.
Which API or parameter should I use to enforce this current limit?
Or is there no callable API, and I need to write my own condition checks?
But since I am in SPEED MODE, is it still possible to impose a current limit?
Thank you in advance to any expert who replies to my question
Solved! Go to Solution.
2025-03-09 9:01 PM
Helo Everybody,
I referred to this article and also tested it. Limiting the Iq current is feasible.
2025-03-09 9:01 PM
Helo Everybody,
I referred to this article and also tested it. Limiting the Iq current is feasible.