2025-07-11 11:24 PM
Hello everyone!
Based on the shot I provided, there are some parameters that I don't know exactly how they are calculated.
What are the Polarization Offset and Offset network attenuation parameters and how could I calculate them? Is there any user guide for that?
It's very useful when designing a custom board
Thank you all
Solved! Go to Solution.
2025-07-16 1:34 AM
Hello @MotorHobbyist,
You can use the embedded tool available on MCSDK5.4.8 Version available here.
Loading "B-G431B-ESC1 electronic speed control" example and clicking on "Analog Input and Protection" and "Calculate" on "Sensing OPAMP" box, a graphical interface pops up that provides amplification chain parameters computation according to resistor values.
2025-07-16 1:34 AM
Hello @MotorHobbyist,
You can use the embedded tool available on MCSDK5.4.8 Version available here.
Loading "B-G431B-ESC1 electronic speed control" example and clicking on "Analog Input and Protection" and "Calculate" on "Sensing OPAMP" box, a graphical interface pops up that provides amplification chain parameters computation according to resistor values.