2012-12-12 03:37 PM
Hi,
I noticed that STM32 MC FOC SDK V3.3 was mentioned in ST Motor Control Workbench V2.1 as one of the target libraries. I also found ahttp://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/RELEASE_NOTE/DM00068242.pdf
mentioning it. But, I couldn't find it being available for download on ST.com. Has it indeed released? If so, where can I find it? Thanks, Tamil2012-12-13 12:50 AM
Ciao Tamil,
The v3.3 is up to now released inconfidential distribution
. So you have to ask it to local ST support office. The WEB distribution will be released soon. Ciao Gigi2012-12-13 01:38 PM
Thanks for the info Gigi!
-Tamil2021-06-21 09:31 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards