2021-03-09 4:02 PM
I am geeting errors when generating the project for EVSPIN32F0601S3, this concludes with: Completed with Errors.
So, when I close the Project Generation, the Workbentch says Generation failed.
I have now changed the location where the projects are being saved, but the following error still present:
2021-03-15 22:21:05,312 DEBUG [LineInfo_to_exitCode.log_LineInfo] 2021-03-15 22:21:05,311 [ERROR] IPConfigManager:1461 - ERROR: the RefConfig ADC_InternalChannelConfig is not available in your config.xml file.
Please advise.
2021-05-25 1:12 AM
Dear @SBung.1
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and SW, CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM MC tools (such as MC_suite, MC-Motor Profile, MC-SDK, MC-workbench, and so on)?
Best regards
Laurent Ca...
2021-05-25 1:28 AM