cancel
Showing results for 
Search instead for 
Did you mean: 

EVSPIN32G4 with MCSDK 6.3.2

Ek92
Associate

Hey, 
I had recently purchased an EVSPIN32G4 board, and I'm currently trying to use the MCSDK to generate code for it.
When I'm trying to generate code for it, it completes with the following error:

Ek92_0-1732018370359.png

How can I solve this issue?

Thanks,
Eyal

1 REPLY 1
GMA
ST Employee

Hello @Ek92,

Differential input is not supported. SingleEnded with internal or external gain topologies are supported.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA