2025-01-31 4:27 AM
Hi Everyone,
Currently I am stuck at place where I want to do some changes in default assigned pin of motor SDK 6.3.2 but unable to do after Version 6.
I was able to do it in MCSDK 5.x.x.. Versions.
if you have any idea about changing pin mapping of ADC sensing pins as well as PWM pins then let me know.
Thanks,
2025-02-03 6:40 AM
Similar problem here.
I created a "Custom board" modifying the pinout and adding "Current sense" funtionality for 3 shunt resistors, and when I want to create a project with that board I only can use 1 shunt.
2025-02-06 6:27 AM
Hello @Akkii,
I assume that you are referring to an Inverter Custom Board?!
Using STMC Board Designer, select "Board kind", on the original board line, select "Clone this item", you will be able to change signal pins configuration.