cancel
Showing results for 
Search instead for 
Did you mean: 

EVSPIN32F601S3 + MOTOR PROFILER

Karan 123
Senior

Hi,

Is there any way to use Motor Profiler with EVSPIN32F601S3 Board ?

--

Karan

1 ACCEPTED SOLUTION

Accepted Solutions
cedric H
ST Employee

Hello Karan,

The EVSPIN32F0601S3 board is based on the STSPIN32F0601 controller which embeds a Cortex M0.

As Cortex M0 does not have FPU, Motor profiler can not be developed for this board.

Regards

Cedric

View solution in original post

5 REPLIES 5
cedric H
ST Employee

Hello Karan,

The EVSPIN32F0601S3 board is based on the STSPIN32F0601 controller which embeds a Cortex M0.

As Cortex M0 does not have FPU, Motor profiler can not be developed for this board.

Regards

Cedric

Thanks.. for update..OK ..

Any other board compatible with NUCLEO-F302R8 for High Voltage BLDC Development . supports Motor Profiler ?

Input voltage from 50 V to 280 V DC/AC

--

Karan

cedric H
ST Employee

All available combinations control + power boards are showed in Motor profiler tool. Click on "select boards" button from the main window to have access to all of them.

Cedric

Ok.. Thanks ..

No Combinations for Input voltage from 50 V to 280 V DC/AC ?

--

Karan

Amit G
Associate II

Were you able get a solution on this?