2020-10-17 2:34 AM
Hi
I am using stspin 3202 six step library to run the bldc motor and using steval3203 board and I am facing this error:
.\Objects\Project_Potentiometer.sct(7): error: L6236E: No section matches selector - no section to be FIRST/LAST.
So how to fix this.
Solved! Go to Solution.
2020-10-26 8:28 AM
Hello @Ryada.1 ,
in addition to set the device as "Standalone" in the Run-Time Environment, verify that the "StartUp" option is checked inside "Device".
Then press Ok in the window and Build the project.
Let me know if this time we fix the error ;)
2020-10-20 12:55 AM
Dear @Ryada.1
According to the rules of the forum with the tag "STM32 motor control", I shorten your title and I move the whole title in the description text part.
Best regards
Laurent Ca...
2020-10-22 1:29 AM
Hello @Ryada.1 ,
are you using Keil IDE?
If yes, you have to set the device as "Standalone" in the Run-Time Enviroment (Project->Manage->Run-time Environment) as shown below:
Let me know if you solved the issue, if yes please "select as Best" my answer.
2020-10-23 10:37 PM
Thanks sir for replay yes i am using keil
2020-10-23 10:43 PM
i did as same you suggested but problem still remain same
2020-10-26 8:28 AM
Hello @Ryada.1 ,
in addition to set the device as "Standalone" in the Run-Time Environment, verify that the "StartUp" option is checked inside "Device".
Then press Ok in the window and Build the project.
Let me know if this time we fix the error ;)
2020-10-28 11:51 PM
thanks for reply sir problem solved thanks a lot sir
2020-10-29 12:35 AM
hi sir i am using motor control workbench generated foc sdk and running motor of 6 pole bldc successfully but in my application of motor heavy load is given on motor so it indicate over current fault so please guide me to by pass overcurrent fault from generated code no matter rpm goes down
2020-10-29 7:10 AM
Dear @Ryada.1
If it is a new question, please open a new thread.
Thanks by advance.
Best regards
Laurent Ca...