2022-03-13 12:59 PM
Hi,
While I was generating a project using ST Motor Control WB v5.Y.4 encountered a problem (attachment). After generating ST Motor Control WB says "Completed with errors". Also when I try to write my own code to control my BLCD motor many vital functions disappear from the libraties generated by WB.
What can I do?
In the attachment I am senging my generation log.
2022-04-06 02:57 AM
Hello @Kamil Wroński,
What I can suggest to you is to generate your project directly from cubeMX.
The MC WB generates an IOC file and ask cubeMX to generate your project from this IOC file.
You will find more details in the following post
Regards
Cedric